Login to your Samtec Service Center
  PRODUCT INFORMATION - Quality Information - Product Change Notifications
Advanced Searches
Below is a list of recent Samtec Product Change Notifications. Click on the "Product Info" link to access Samtec's Technical Specifications which include prints, footprints, and catalog pages for that series.
DATE
SUBJECT
PRODUCT
INFO
08/08

Effective September 1st 2008, Samtec will no longer offer the screw machine terminal T-1R13-G or T.

The sales on this lead style were very low and only a small number of customers were affected.  I will be forwarding a list of customers to those rep organizations, territory managers or country managers with customers who are affected by this update.  Samtec will honor existing orders through August 31st.

New orders will be accepted based on availability of material so check with your customers on their usage through August 31st.

 
07/08

Effective immediately, Samtec will no longer offer the SSK Series.  If you have a customer who wishes to purchase the SSK Series, please inform them that the SSA, SLW and CES Series are possible replacements.  The SSA accepts .015” (.38mm) to .022” (.56mm) diameter lead and most IC leads.  The SLW and CES will accept a .025” (.64mm) square lead.

 This original cutoff date for the SSK Series was December 31, 2007, but we allowed orders to continue.  I will be forwarding a list of customers to those rep organizations, territory managers and country managers with customers who are affected.

 
07/08

A Keyed Polarization option has been added to the IPL1 -K, SCR2 -DK, MMSD -K, MMSS –K and IPD1 -K Series as a required callout on all new customer designs.  This Keyed Polarization Option will eliminate a customers concern of miss mating of an IPL1 to a MMSD as one example.

The Keyed Polarization option does not change the fit, form or function of the series listed above.

Here is a link to updated catalog pages that have also been added to the web:

 ftp://ftp.samtec.com/webfiles/pdf/scr2.pdf

 ftp://ftp.samtec.com/webfiles/pdf/mmsd.pdf

 ftp://ftp.samtec.com/webfiles/pdf/ipl1.pdf

 This will not affect existing customers because those customers will be allowed to continue to purchase the older version.

 
07/08

The QRM8 and QRF8 Series callouts have changed to QEM8 and QEF8.  Here are links to the updated catalog pages that have also been added to web. 

ftp://ftp.samtec.com/webfiles/pdf/qem8.pdf

ftp://ftp.samtec.com/webfiles/pdf/qef8.pdf

There is no change to the fit, form or function of the part.  The estimated release of these series is August. 

 This change will allow Samtec to use the QRM8/QRF8 series name for future expansion of the Q-Rate product line. 

 
05/08

The -01BJ2 end option has been released for sale for the RF174, RF178 and RF316 cable assemblies.  This end option has been added to the catalog pages and placed on the web.  Here is a link to these pages:

http://www.samtec.com/ftppub/pdf/rf174.pdf

http://www.samtec.com/ftppub/pdf/RF178.PDF

http://www.samtec.com/ftppub/pdf/RF316.PDF

 

 
04/08

The minimum number of positions for the –P (Plastic Pick-n-Place Pad) option offered in the catalog has changes from 5 to 6.  Here is an updated catalog page already loaded to the web:

Customers can order smaller sizes, but must contact Samtec first for availability.

04/08

With the upcoming addition of a loose contact version of the T-1M44 Series, Samtec has modified the callout to include this new option.  Here is a breakdown of the new callout:

T1M44-R-2830-01-H (Full Reel)
T1M44-L-2830-01-H (Loose Contact)

03/08 We have made an update to the cable length of the FFTP/FMTP. The -08.84 length callout has changed to -08.87.
03/08

The good news is we have an improved, more intuitive part numbering system for the Q2 product line.  The good news is our existing current customers do not have to change their part number.

Effective immediately, Samtec is updating the lead style callouts on the QMS, QFS, QMSS and QFSS Series.  The new lead style callouts, when added together, equal the board spacing distance of the Q2 system.  This makes it easier to design-in and select the right socket and terminal combination. 

This change does not affect existing customers; they will be allowed to continue to order the current lead styles.  This change also does not affect the QMS/QFS right angle or edge mount options and QMSS edge mount option.

Here is a breakdown of the change:

                              Current                  New

Series                   Lead Style         Lead Style

QMS/QMSS            -10                     -05.75

QMS/QMSS            -11                     -06.75

QFS/QFSS               -01                    -04.25

03/08

Samtec is in the process of expanding the MODS-LJ Series to include LED options and In-line multi banks.  Due to the addition of these new options, Samtec is updating the MODS-LJ Series part number call out that is currently in the F-207 Full Line Catalog.  

03/08

The RSEAF Series will not be released and has been removed from the F-208 catalog due in the next two weeks.  The SEAF-RA, which uses a wafer instead of a flex cable in the RSEAF, will have a better performance with lower cost.  The estimated release for sale of the SEAF-RA is 4th Quarter 2008 with samples available the end of Summer.

03/08

The SCPC/SCRC Series will not be released.  Please mark this series out of your F-208 catalog page 189.  This series will be removed from the F-208-1 catalog due for release September/October of this year.  A re-design version is in the works but has a mid 2009 estimated completion.

 
02/08

Effective July 1st 2008, Samtec will no longer offer the screw machine socket SC-2P2 and screw machine terminals T-1R14-04 and T-1R14-05. 
Here is a list of the series and their lead styles effected:

BBS, BHS, BBD - lead style D and G
AP, APA, APS - lead style Q
SS. SD, BHS - lead style 9
IC, ICA, ICS, ICE - lead style H. 

BBS, BHS, BBD, AP, APA, APS, SS, SD, BHS, IC, ICA, ICS, ICE
Product Change Notification Archive. top