Geek Speek Webinar — Mechanics of Using the Public COM Code

Presented by: Richard Mellitz Channel Operating Margin (COM) is an electrical figure of merit for a channel derived from a measurement of its scattering parameters and a table of configuration parameters. These parameters may be represented as a machine readable form in a spreadsheet. COM is normative for many IEEE and OIF specification for data rates over 25 Gb/s. COM is described in Annex 93A of IEEE Std 802.3™-2018. An example of a COM implementation is available as a Matlab® script. The subject of this presentation illustrates the operation of the COM script as well as exploration of features of the many parameters and control keywords. The example of using COM explores the required reference packages and then segues into examples and caveats for utilizing the COM script with user packages. Operation are depicted as example screen shots.

(This is the second in a series of blogs, from Sandeep Sankararaman, Samtec’s Principal RF and Signal Integrity Engineer, discussing design strategies for high-bandwidth RF launches. The first is entitled “What Is An RF Connector Launch?” The third, coming next week, discusses GN...
If you’ve been paying attention to the Coming Soon section in our most recent web updates, you might have noticed we have been working on an upgraded Checkout system for the website for the last several months. We’re happy to announce that this application is now accepting orders...
As signal speeds increase, each part of the signal path getting to and from the device needs to work to higher frequencies.  Strategies that worked in the past no longer suffice and cheaper connectors no longer make the cut. Cable lengths and trace lengths need to get shorter to ...
This month, we released a major new version of our Checkout to a beta state, made some upgrades to how we show lead times online, made 3D model downloads easier from the Search, and released a few more content updates. Here are the major website updates to Samtec.com for July 202...
Something occurred to me recently. AI hardware system architectures are really applications-specific. Computing platforms from laptops, desktops, workstations and servers follow classical architectures. Inputs, outputs, a central processing unit, busses (control, data and memory)...