FQSFP-DD SI评估套件

FQSFP-DD SI评估套件

适用于评估FQSFP-DD系列双倍密度Flyover® QSFP28电缆系统的SI测试平台


概述

随着数据速率的增加,PCB上的线路长度会减少。Samtec的高速Flyover®电缆组件简化了PCB设计,并限制了高数据速率应用中的信号衰减。FQSFP-DD SI评估套件为系统设计人员和SI工程师提供了测试FQSFP-DD系列双倍密度Flyover® QSFP28电缆系统(包含各种终端2选项)的一种易用型解决方案。

FQSFP-DD到AcceleRate® Flyove® SI评估套件 (REF-203424-X.XX-XX) 通过高精度射频连接器、FQSFP-DD到AcceleRate®电缆组件和PCB安装连接器路由八个高速差分对。

FQSFP-DD到DCH Flyove® SI评估套件 (REF-203423-X.XX-XX) 通过高精度射频连接器和FQSFP-DD到DCH电缆组件路由八个高速差分对。

FLYOVER REF203424
Samtec零件编号REF-203424-X.XX-XX,如图

FQSFP-DD SI评估套件提供具有强大机械设计的高质量系统。有关更多信息,请通过KitsAndBoards@samtec.com 联系Samtec的技术专家。

特色

  • 一套FQSFP-DD系列双倍密度Flyover® QSFP28电缆组件
  • 支持多种FQSFP-DD系列电缆长度选项
  • 支持多种高精度射频连接器选项 (2.4 mm/2.92 mm SMA)
  • 通过Samtec FinalInch® BOR PCB追踪路由优化的‘SI性能
  • 通过直接连接到TDR/TDT来启用时域测量
  • 通过直接连接到VNA来启用频域测量

应用

  • 服务器
  • 存储
  • 网络
  • 测试和测量
  • 有线通信
  • 无线通信

订购信息

更多详情,请参见图样REF-203424-X.XX-XX and REF-203423-X.XX-XX

联系销售

电子邮件
公司
行业
预计年用量
系列
消息

不想填表格?
直接与产品专家在线聊天

.
.
Many electronics experience a wide range of climates while in operation and storage. Because of this fact, connector humidity testing is used to determine the ability of a product to withstand elevated humidity and cycling temperatures. Humidity testing is conducted in combinatio...
In this new video, Samtec’s Kevin Burt introduces Samtec Direct Connect™. Direct Connect gives the benefit of exiting a higher number of lanes at low loss from the chip package, which can be very useful in both high performance computing and network switching applications, especi...
This is the first release of a few phases of a new login system for Samtec.com. This replaces a system that was built in 2011 and has been running well ever since. But, technology changes over time, and it was time for an upgrade. Here are some additional details about the featur...
Modern electronic devices are getting smaller with every new generation, and as a result, they are becoming more portable.  At the same time, the performance of these devices is growing as the demands of consumers become greater.  We expect to be able to connect to the internet w...
This month, we released a major upgrade to our login experience across Samtec.com, as well as an overview of our 5G technology capabilities, and an easier way to get real-time availability for products across Samtec.com. Here are the major updates to Samtec.com for July 2019. Rea...