NovaRay® I/O 112 GbPS PAM4面板安装电缆系统

NovaRay® I/O 112 GbPS PAM4面板安装电缆系统

NovaRay® I/O运用Flyover®电缆技术,可将高达3,584 Gbps PAM4的总数据从IC封装路由到面板等组件。


系列概述

NovaRay® I/O提供市面上最高的总数据速率3,584 Gbps PAM4,采用高密度电缆到电缆隔板连接。Flyover®电缆技术通过有损PCB路由数据,从而简化电路板布局并扩展信号范围,包括盒内和盒外。无源外部电缆可防止面板产生大量热负荷,并且不需要散热器,节省了宝贵的面板空间。

NovaRay I/O

特色

 

  • 16 & 32差分对配置
    • 容纳PCIe® x4或x8+边带
  • 使用Flyover®电缆技术的电缆到电缆隔板连接
  • 外部电缆:28或34 AWG双芯
  • 内部电缆:34 AWG双芯
  • 还提供单端同轴选择
  • 外部全EMI防护
  • 提供耐用型38999外壳,可抗盐雾达48小时,具有IP67密封选项 (NVA3E/NVA3P)
  • 为您的ASIC相邻Flyover®互连器提供多端2高速连接器选择
兼容pci express第6代

终端2选项:

novaray
高密度、细长型电缆组件
  • 8、16或24个差分对
  • 垂直和直角配置
  • 支持高达28G NRZ/56G PAM4的所有信号协议
arf6对接电缆 56 gbps
novaray
高密度阵列电缆组件
  • 8至32个差分对
  • 垂直配置
  • 支持高达56G NRZ/112G PAM4的所有信号协议
arf6对接电缆 112 gbps
novaray
轻薄型电缆组件
  • 8或16差分对
  • 直角配置
  • 支持高达56G NRZ/112G PAM4的所有信号协议
arf6对接电缆 112 gbps

超低偏斜双芯电缆

Samtec的独家共挤式低损耗双芯电缆技术消除了单挤介质双轴电缆的性能限制和不一致性,改进了信号完整性、增加了带宽和覆盖范围。

  • 尤其适用于28-56+ Gbps应用
  • 信号导体之间的紧密耦合
  • 超低偏斜双芯光缆 < 3.5 ps/meter
  • www.samtec.com/flyover
arc6 flyover

下载和资源

资料

高速电缆互连方案指南

高速电缆互连方案指南

下载PDF文件
高速电缆互连方案指南

高速电缆互连方案指南

下载PDF文件

技术文档

产品

NVACE

NovaRay® I/O极致性能电缆组件

特色
  • 外部,盒外电缆
  • 使用Flyover®电缆技术的电缆到电缆隔板连接
  • 高达3584 Gbps PAM4的总数据速率
  • 112 Gbps PAM4在16和32对配置中的性能
  • PCI Express® 6.0解决方案的x4和x8对配置
  • 28或34 AWG双芯电缆;34 AWG同轴电缆(可用单端信号)
  • 耐用型外部屏蔽提供EMI保护
NovaRay® I/O极致性能电缆组件

NVACP

NovaRay® I/O极致性能面板安装电缆组件

特色
  • 内部,盒装电缆
  • 使用Flyover®电缆技术的电缆到电缆隔板连接
  • 高达3584 Gbps PAM4的总数据速率
  • 112 Gbps PAM4在16和32对配置中的性能
  • PCI Express® 6.0解决方案的x4和x8对配置
  • 28或34 AWG双芯电缆;34 AWG同轴电缆(可用单端信号)
  • 耐用型外部屏蔽提供EMI保护
NovaRay® I/O极致性能面板安装电缆组件

NVC

NovaRay® I/O压铸面板外壳

特色
  • 提供1、2或4端口配置
  • 用于EMI面板保护的弹簧触片
  • 设计用于NVACP面板安装电缆组件
NovaRay® I/O压铸面板外壳

联系销售

电子邮件
公司
行业
预计年用量
系列
消息

不想填表格?
直接与产品专家在线聊天

.
Samtec Harrisburg attended the 17th annual Penn State Harrisburg Signal/Power Integrity Symposium and MASH Forum on Friday, April 19th 2024, hosted by the Center for Signal Integrity. The main goal of the […] The post Samtec Design Center Attends Annual Penn State Harrisburg SI/P...
As the world gears up to celebrate the 150th running of the Kentucky Derby,the excitement is intense. This iconic event isn’t just about horse racing;it’s a celebration of tradition, athleticism, […] The post Celebrating Community and Innovation: Samtec’s Connection to the 150th ...
Wait . . . An AI hardware platform without a GPU? Is that even possible? Obviuolsy, I jest. GPUs are the workhorse solutions for ever larger LLMs and cutting-edge generative […] The post New AMD Versal AI Edge SoM and Carrier Card From Avnet Feature Samtec Interconnects appeared ...
Artificial Intelligence. Or, the intelligence of computers. It’s all around us, but I think it’s important to remember that this intelligence is driven by human intelligence. It’s the human innovation behind […] The post Artificial Intelligence: How to Manage High Amounts of Dat...
Our modern industrial world depends on raw materials. Whether oil, steel or cotton, raw materials have been of huge importance to the development of the industriaized world. While these physical […] The post Connectors for HPC and Supercomputing appeared first on The Samtec Blog....