该COBO(板载光学元件联盟)的子规范定义了COBO合规板 (CCB) 的特性,它用于COBO网络设备的电气和光学测试。CCB包括主机合规板 (HCB) 和模块合规板 (MCB),它们均支持400GAUI-8 C2M接口。

COBO光学元件标识

HCB-MCB合规板

FireFly™

COBO连接器系统具有灵活性、出色的信号完整性和经济高效的设计,是板载光学元件应用的理想选择。它包括用于高速功能的插卡式连接器和用于管理接口和电源端子的单片式z轴连接器(改进的SamtecUCC8闭锁插座)。

高速插卡式连接器专用于支持×8和×16通道要求。连接器系统的信号完整性 (SI) 性能支持COBO在56 Gbps PAM4信令下的操作要求。

Cobo
UCC8

联系销售

电子邮件
公司
行业
预计年用量
系列
消息

不想填表格?
直接与产品专家在线聊天

.
Nvidia had its annual GTC gathering of AI developers, fans, media, and gamers recently. The newly announced Nvidia Blackwell platform is scheduled for release in late 2024/early 2025. Blackwell will […] The post From AI to SI: Samtec Participates on Two Upcoming Webinars appeared...
There are several Advantages of Being a Samtec Co-Op, but at the heart of the Samtec Co-Op program, the main goal is to foster, nurture, and provide engaging, hands on […] The post An Interview with Business Co-Op’s at Samtec appeared first on The Samtec Blog....
OFC, the Optical Fiber Communications Conference, is all about optical networking and communications. Samtec was front and center showcasing 224 Gbps PAM4 solutions, next-generation transceivers for optical and copper, CXL-over-optics, […] The post Cutting Edge Copper and Optical...
Designing and optimizing a breakout region (or component launch) for a connector can be challenging. It often requires multiple back and forth iterations and analysis to adjust variables. Samtec’s new […] The post How to Design Component Launches Faster appeared first on The Samt...
It’s that time of year again. The world of CoMs, SoMs, interconnect and more all converge next week. The world of embedded systems is multifaceted – from hardware and software […] The post Guten Tag! Visit Samtec at embedded world 2024 in Nuremberg appeared first on The Samtec Bl...